1/27/2014 10:02 AM | |
Posts: 3609 Rating: (29) |
Import of a Technical Question of the User NuTriStAr
|
1/27/2014 11:22 AM | |
Joined: 4/22/2010 Last visit: 11/18/2024 Posts: 5697 Rating: (715)
|
Hello, Yes you can downgrade a CPU firmware by "upgrading "with older firmware. Your older CPU can also be upgraded, but then your CPU will stop. You find the Upgrades here: Operating System Updates: CPU412-3H / CPU414-4H / CPU414-4H PG / CPU417-4H and CPU412-5H PN/DP, CPU414-5H PN/DP, CPU416-5H PN/DP, CPU417-5H PN/DP I would downgrade the 2nd CPU and when you can stop the plant upgrade both.
Regards, Marcjan |
Last edited by: Marcjan at: 1/27/2014 11:37 AMProblem solved? |
|
This contribution was helpful to1 thankful Users |
1/28/2014 10:01 AM | |
Joined: 6/8/2013 Last visit: 8/4/2024 Posts: 14 Rating: (0) |
Thank you for the information. But when I click on the following file to extract it I get this error. I dont know what it means but do you have any other links to get the V4.0.7 OS firmware update. Please see attachment for the error that appeared when clicking the file. |
1/28/2014 10:49 AM | |
Joined: 4/22/2010 Last visit: 11/18/2024 Posts: 5697 Rating: (715)
|
Hello, The message tell the archive is corrupt, it is not, i could download and extract it without any problem. I zipped the data again and attached it here. To download it you must be logged in. Hope this works. Regards, Marcjan Attachmentfirmware.zip (396 Downloads) |
Problem solved? |
|
Follow us on