5/6/2008 5:47 PM | |
Joined: 3/2/2008 Last visit: 1/9/2009 Posts: 8 Rating: (3) |
It is often necessary to start up a Simotion system without all the Drive-Cliq+ connections available. The best way to proceed is to Deactivate the Servo or Vector entries that are not available. A drive is deactivated by setting p105 to zero. I've attached a rather handy S120 script file for asking you if you'd like to deactivate drives and automatically setting p105 to zero for each drive in the project. You'll notice this script is written for V2.5 version drives. This script can be easily modified for V2.4 or older projects if you normally start up your Simotion system without all drives available AttachmentDisable p105.zip (780 Downloads) |
Follow us on