11/19/2024 10:32 AM | |
Joined: 10/12/2023 Last visit: 9/16/2025 Posts: 120 Rating:
|
Hi.
Upgrade Roadmap (V7 Engineering Help) The upgrade roadmap provides you with high-level tasks that are required to upgrade the Management Station along with all the installed prerequisites, language packs and extensions with the post-installation steps, if any. In Version 7.0, upgrade is supported only for Desigo CC Version 5.0 and above.No interim upgrades are supported. For example, upgrade from lower build number to higher build number of Desigo CC Version 7.0 is not supported. https://sid.siemens.com/r/A6V14198387/22837779723_22838076171__en-US_15175607307 Update Desigo CC application Just used to add extension modules and/or language packs of the same Desigo CC version. It is therefore not the same as the Update button you know from other applications that allows you to update the application to the latest version. |
Last edited by: Chris_PL at: 11/19/2024 10:35:22Best regards, |
|
11/20/2024 7:17 AM | |
Joined: 1/30/2019 Last visit: 9/5/2025 Posts: 71 Rating:
|
problem solved, it was due to the firewall |
12/10/2024 9:14 AM | |
Joined: 3/11/2021 Last visit: 9/12/2025 Posts: 3 Rating:
|
Can you tell me what exactly happened with the firewall, as I have a similar problem on version 3.0? |
Follow us on