8/28/2025 9:44 AM | |
Joined: 7/15/2022 Last visit: 9/2/2025 Posts: 10 Rating:
|
Hi, I got an installation that need to communicate with a other, external installation. A PN/PN Coupler makes the bridge between both installations. When my installation is powered off during a while ( during a whole week-end, for exemple) I got the Siemens ID 16#06:4040 and 16#06:4000. This is True until I make a Stop/Run at the PLC (1512 SP). Thats the only situation where this problem happen's. The Diagnose Buffer tells me to check the connection on the coupler, but those are good. ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 08/28/2025 12:11:50New subject after splitting |
|
Follow us on