7/13/2009 9:43 AM | |
Posts: 89 Rating:
|
What is the meaning or fullcform of DP/AS-i-link and what is this?????? |
7/13/2009 12:47 PM | |||
Joined: 9/27/2006 Last visit: 6/27/2024 Posts: 12263 Rating:
|
Hello mohit; I hope I understand your question correctly. You must make an effort to be clearer, and give more details: what do you need the module for, what type of project do you plan to use it in... In any case: The DP/As-i link is a communication gateway provided by Siemens so data from an As-i network can be transfered over a Profibus-DP bus to the CPU. This is useful when you already have a Profibus-DP network, and you do not want to put a As-i master card in the CPU rack. Siemens calls these elements "network transitions"; they provide for example DP/DP couplers, DP/RS-232 links, DP/PN proxys.... Here is some further information on the DP/As-i link: From the A&D Mall:
Click on the hyperlink aboveand access the “Description” tab for more details. Product description:The DP/AS-Interface Link 20E (6GK1 415-2AA10) connects PROFIBUS DP with AS-Interface. It features the following functions: • PROFIBUS DP slave and AS-Interface master • Connection of up to 62 AS-Interface slaves and integrated analog value transmission (according to extended AS-Interface Specification V3.0) • Support of all AS-Interface master functions according to AS-Interface Specification V3.0, i.e. master profile M4 • LEDs on the front panel to indicate the functional readiness of the connected AS-i slaves and to display the status (configuration mode, AS-Interface power failure, configuration errors, etc.) • Supplied from the AS-Interface line; therefore no additional power supply required • Supports uploading of the AS-interface configuration in STEP 7 V5.2 or higher Hope this helps, Daniel Chartier |
||
Last edited by: dchartier at: 7/13/2009 12:52 PMIn case your enquiry was about the As-i network, here are some links you could look at: As-I products from Siemens: https://www.automation.siemens.com/cd/as-interface/html_76/products.htm As-I technical information from As-interface.net: http://as-interface.net/System/ |
|||
This contribution was helpful to
1 thankful Users |
7/13/2009 9:22 PM | |
Posts: 89 Rating:
|
Thankyou dchartier this knowledge is sufficient for me |
Follow us on