7/12/2014 2:14 PM | |
Joined: 10/11/2006 Last visit: 8/29/2025 Posts: 6037 Rating:
|
Hello, now the new blocks are available for S7-1200/1500 AND S7-300/400: http://support.automation.siemens.com/WW/view/en/68034568 |
With best regards, |
|
7/12/2014 10:36 PM | |
Joined: 5/22/2012 Last visit: 3/24/2022 Posts: 895 Rating:
|
Hello, have you read the documentation really? All blocks are explained and with timing diagramms. If you have idea`s/improvements for the documentation, there is a button Suggestion for the entry. If you prefer to use PLC Open blocks for programming, you can use S7-1500 with the so called "Technology objects". Thisis really a very user friendly way, but from my side, I prefer the setpoint interpolation (ramp generator) inside the drive, because I use the calculation power for the setpoint generation on the drive side. You can use the drive-lib, or using standard communication with SFC14/15 (DPWR_DAT / DPRD_DAT). Following you have the structure of each standard telegramm as a UDT: http://support.automation.siemens.com/WW/view/en/82841762 Best regards Zako |
7/14/2014 4:29 PM | |
Joined: 10/11/2006 Last visit: 8/29/2025 Posts: 6037 Rating:
|
Hello, I don't know your solution. Here is a link to a ready example for comparing. http://support.automation.siemens.com/WW/view/en/70155469 |
With best regards, |
|
Follow us on