5/8/2025 10:06 AM | |
Joined: 9/27/2006 Last visit: 9/8/2025 Posts: 12401 Rating:
|
Hello Eugeniusz_G; What voltage level do your computer run on? As you can see in this link to the UPS1600/BAT1100 systems, they provide extended power to 24 VDC units, eg PLCs. https://support.industry.siemens.com/cs/ca/en/view/109978735/182394125707?dl=en If you need 120/230VAC UPS, maybe it would be more efficient to source a reputable local vendor of the type of equipment you require, to ensure their help in the design and support of the selected UPS. Hope this helps, |
5/8/2025 10:36 AM | |
Joined: 9/26/2019 Last visit: 5/8/2025 Posts: 2 Rating:
|
I need a device with 24V DC power supply. |
5/9/2025 12:17 PM | |
Joined: 9/27/2006 Last visit: 9/8/2025 Posts: 12401 Rating:
|
Hello Eugeniusz_G; If that is the case, the Sitop UPS 1600, with supporting battery modules, can probably help you. See the image below, taken from this document on different Sitop UPS models. https://support.industry.siemens.com/cs/de/en/view/109765862 You already have a link for the UPS 1600 system manual, you can look up the Specifications section to see details of the required 24 VDC input connections and see what 24 VDC output power and buffering the different models of the UPS 1600 can offer to your PC. Hope this helps, Daniel Chartier |
Last edited by: Moderator_Lan at: 05/09/2025 12:24:52link optimized Last edited by: dchartier at: 05/09/2025 13:31:58 |
|
Follow us on