4/1/2016 4:00 AM | |
Posts: 5 Rating: (0) |
I'm a failure in AFE 029, but it only appears when the command is off, aproximandamente five minutes later, remaining until the command is on holding the reset button, and tighten the control on the crane. I made the measurement of CT's, through TESTBOX, and the phase CT W (L3) is to offset values outside the standards in Ohms! If the problem really is the CT, then it is still sending feedback to the ABO, and thus for the IVI board, even after you have turned off your command? And as he does not have this flaw when it is connected in operation? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/1/2016 10:36:32 AMNew subject after splitting Last edited by: Min_Moderator at: 4/1/2016 10:37:40 AMAdd second topic |
|
4/1/2016 10:41 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
Closed cause question posted twice. The second thread with the subject CU 029 has a failure is published within the conference SIMOVERT MASTERDRIVES. Best regards Min_Moderator |
Follow us on