4/15/2016 4:25 PM | |
Posts: 23 Rating: (0) |
Will check tommorow morning. |
4/16/2016 4:05 AM | |
Joined: 10/17/2007 Last visit: 5/30/2024 Posts: 3992 Rating: (345) |
Hi, did you also post this? https://support.industry.siemens.com/tf/de/en/posts/810d-pcu20-feed-and-spindle-problem/146085/?page=0&pageSize=10 if you are looking for solution for same problem, I suggest don't focus on "Feed enable" on the machine control panel. I attached picture, which is from my shop m/c DMG "Twin 65" turning m/c. after I read you post, I just went to try that red color key (left side part 3rd line from bottom) seems like "Feed Disable" button, even I press and hold it, but no use, I can still jog X,Z,... As I know Not all OEM/m/c builders following Siemens idea. I am trained by Siemens and most time followed its idea. when I design or rebuild m/c PLC program for customer, I always use Siemens standard MCP, and use "feed on/off" "spindle ON/OFF" keys on it. But m/c builder , such as DMG, Index, they don't like that , --you see --Siemens should follow them. the machine control panel in your and my pictures are Siemens special made for DMG. Index not use Siemens MCP at all, As I know these 2 OEM's they don't use "Feed ON" button function, after m/c power up, if all condition meet, all feed/axis will automatic enable--otherwise, there is some thing wrong to disabled feed. So take more time to look for why you have alarms and feed/axis not moving. the best way is to ask DMG or former m/c owner. another solution is diagnosis by PLC--if you have SIMATIC Manager in PC and possible online.
|
If you like my comments please |
|
4/16/2016 8:51 AM | |
Posts: 23 Rating: (0) |
Hi there, Thanks for your detailed answer. problem occurs for feed is because i can not put main spindle in reference position, axis X, Z, C1 are referenced, only problem is C4 (c axis for milling and S axis for turning) thats why i cant move feed or maybe spin this axis in desired speed, But i dont know why its happening i run machine, transfered programs etc etc, make cutting, turned it off and i couldnt refer my spindle, i think thats main problem with machine. In attachment you can find NC.arc and PLC.arc file AttachmentNC.zip (130 Downloads) |
Follow us on