9/28/2021 12:15 PM | |
Posts: 257 Rating: (75)
|
We are receiving more and more questions regarding the current configuration of the SIMATIC Field PG M6. The configuration of a SIMATIC Field PG M6 can be created in the TIA Selection Tool. At the moment, only TIA version V16 can be selected. A changeover to V17 is in progress. Until the changeover has taken place, all SIMATIC Field PGs manufactured from now on will automatically contain the corresponding V17 licences, as the TIA Portal V17 has already been released for delivery. At the same time, the SIMATIC Field PG M6 also includes the installation DVDs for TIA Portal V17. The pre-installed software and the restore DVDs remain with V16. Note The procedure described in this article refers to the time when this article was written (status: August 2021). With Best Regards, SIMATIC International Technical Support Hub
|
Follow us on