3/19/2025 5:19 PM | |
Joined: 7/25/2022 Last visit: 3/24/2025 Posts: 5 Rating:
|
For example, the AK2DG from Kollmorgen. I will attach the GSD file The intention is to map the standard telegram 0 ("ID_ProfiDrive_ST0" in the gsdml) and select the inputs and outputs using the standard profidrive parameters p915 and p916. AttachmentGSDML-V2.43-KOLLMORGEN-AKD2G-20241024.zip (247 Downloads) |
3/19/2025 6:14 PM | |
Joined: 9/21/2012 Last visit: 9/10/2025 Posts: 4708 Rating:
|
The parameter writing part is addressed in the manual 3.6 Parameter Configuration with PROFIdrive over PROFINET IO. |
Follow us on