10/13/2011 1:02 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Did yopu receive any errors? Best regards, Hristo Mihalev |
10/13/2011 1:05 PM | |
Posts: 36 Rating:
|
yes i recieve an error |
10/13/2011 1:08 PM | |
Posts: 270 Rating:
|
Hello Zee.Alam, do you get any sort of error while this happens or is there any sort of indications in the log file? Also, there is a thread regarding this topic (/tf/WW/en/Posts/23960), where some user suggests to create a new project and paste into it the whole previous project (however, that might be a problem if you only got 2008). |
Last edited by: MM1234 at: 10/13/2011 1:09 PMDid you receive any errors? ... Yes, I did. ... LOL, that totally got me, hahaha :) |
|
10/13/2011 1:14 PM | |
Posts: 36 Rating:
|
this is the first message |
10/13/2011 1:15 PM | |
Posts: 36 Rating:
|
this is the error |
10/13/2011 1:18 PM | |
Posts: 36 Rating:
|
i have installed hot fix 1,2,3.. but still the same error |
10/13/2011 1:20 PM | |
Posts: 270 Rating:
|
The error says that you find details in the logfile, so perhaps really paste here the logfile, so someone can help you ;] |
10/13/2011 1:24 PM | |
Posts: 36 Rating:
|
okie |
Follow us on