4/21/2025 10:22 AM | |
Joined: 1/21/2025 Last visit: 4/21/2025 Posts: 3 Rating:
|
Hello, I havr this error ,i need solution |
4/21/2025 10:37 AM | |
Joined: 5/6/2022 Last visit: 7/10/2025 Posts: 589 Rating:
|
Hi AutoGen_9315175, From the error message you share it looks like the project is damaged or faulty. It looks like the SQL database of the project may be corrupted. In this case, it would surely have to be checked from Siemens technical support whether it can be repaired or not. In many other cases, that I have seen with this error, unfortunately it could not be repaired. Still, you could try to ask them. Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
4/21/2025 10:49 AM | |
Joined: 1/21/2025 Last visit: 4/21/2025 Posts: 3 Rating:
|
Thank you for answering me, but the same project works on my friend's normal PC. |
4/24/2025 2:01 PM | |
Joined: 8/3/2009 Last visit: 9/5/2025 Posts: 16349 Rating:
|
Hello Which exat Version of WinCC flexible do you have (with SP and Upd)? Which OS do you use? Check this FAQ: https://support.industry.siemens.com/cs/de/en/view/29420407 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on