1/20/2023 8:13 PM | |
Joined: 9/9/2022 Last visit: 10/27/2023 Posts: 11 Rating:
|
Hello! I'm also having the same problem. I'm using a SM 1278, 4 X IO-LINK MASTER (6ES7 278-4BD32-0XB0 V2.1) and on Port 2 of the IO Link Module I have a Siemens 8WD4613-5HH47 Light Tower. I'm getting error code 8601. I've attached my function block. I got the hardware ID from the "system constants" of the IO Link module. Is that the correct hardware ID? I noticed you used 1 as the hardware ID. That indicates the OB Main in the system constants of my PLC. Is 127 correct on my end? ------------------------------------------------------------------------------------------ |
Last edited by: Icky7a at: 01/20/2023 20:45:25Last edited by: Jen_Moderator at: 01/23/2023 04:44:24New subject after splitting |
|
This contribution was helpful to
1 thankful Users |
Follow us on