2/25/2011 5:49 PM | |
Joined: 11/18/2009 Last visit: 3/22/2021 Posts: 14 Rating:
|
Hi, Is it possible to have different hardware configuration in the CPU 0 and CPU 1 in a 400-H system? Say I down load hardware config to reserve CPU in STOP mode and switch ON without switch with altered config option what will there be any error? Regards, Arunkumar Splitted from how to download program in 400-H system. |
Last edited by: O_Moderator at: 2/28/2011 9:19 AMnew subject after splitting |
|
2/28/2011 1:02 PM | |
Joined: 11/18/2009 Last visit: 3/22/2021 Posts: 14 Rating:
|
Hi Greg, thanks a lot. |
3/2/2011 3:04 PM | |
Posts: 947 Rating:
|
As sample see02/2009 A5E00267695-06 on page 123 (paragraph 10.3 Using single-channel, one-sided I/Os) |
3/9/2011 6:52 PM | |
Posts: 947 Rating:
|
Hello, Arunkekkar I have about 4 years have not worked in detail with the H-system, so I could be wrong (if anything, sorry). I will describe his vision of the H-system. When the processor is empty (for example, after the M-res), then when you load a program into a single CPU (eg, 0), then sync software modules loaded in a different CPU (1). Thus automatically obtain the same program in both the CPU. (Possible adjustment programs occurs when you run the processor). This explains the fact that as a result of your comparison of programs, you do not find differences. However, if you changed the configuration and load it into the CPU, then the equalization program to 0 and 1 CPU is no longer happening. To avoid problems associated with varying configurations and programs, I always post any changes laden programs in both CPU. I use Google-translate , and maybe something or misunderstood, ortranslate into English. If it is not clear, then ask. Regards, gre_m |
3/9/2011 7:32 PM | |
Joined: 11/18/2009 Last visit: 3/22/2021 Posts: 14 Rating:
|
Thanks |
Follow us on