9/15/2017 10:36 AM | |
Posts: 6 Rating:
|
Hi, I have an issue with downloading the OPC (TIA Portal) to the PC (Industrial PC). In the TIA, everything is ok and I tried even the same program of the last machine which worked well but the problem is that PC doesnt show in the TIA. When I go to the Online access, click on update accessible devices and he says that there is no device, followed by System Error (Message 140:511). Could someone please assist me in this issue. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/19/2017 7:33:13 AMNew subject after splitting |
|
9/15/2017 3:14 PM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello Haydoo Im not sure what you want to do exactly -> So first of all we need more information like: - Which exactTIA Portal Version? - Which Simatic Net Version do you have on Runtime PC? - A Screenshot of the Error Message? - Which PC or IPC do you use? - Screenshot of the Device View and the Network View in TIA Portal - Screenshot of the Component configuration on the Runtime PC - Do you use xdb File for configuration ? Look here for a general overview: http://support.automation.siemens.com/WW/view/en/13542666 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on