4/9/2025 7:41 PM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi Cmac987, So you now have some script like:
Since you are using the Trace method, have you already checked what the Trace Viewer displays? Are you sure the SD card is available to the system? You can use the File Browser app to check whether the SD card is visible there. Please also note that the data you write to the file is buffered by the operating system. It takes some time for the data to be physically written to the SD card. Since Unified Comfort Panels do not offer a reliable way to safely eject the SD card, you should only remove it after restarting the system to ensure that all buffered data has been written. Kind regards |
4/14/2025 11:11 AM | |
Joined: 8/3/2009 Last visit: 9/2/2025 Posts: 16290 Rating:
|
Hello Cmac987 The 2GB SD Card from Siemens has a special file system, if you format it you cannot use the advantages any more (and you cannot use this also for Systemcard in WinCC Comfort Panels after that): https://support.industry.siemens.com/cs/ww/de/view/95853895 -> try the way from the FAQ for clearing the Card. Check if you do not have switched the hardware write protection switch on the Card. Perhaps then it work Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on