3/25/2022 10:38 AM | |
Joined: 2/10/2022 Last visit: 1/9/2024 Posts: 42 Rating:
|
Hello guys, i have arrieved to your post and im having so problems near to it. First of all is, its possible to reduce the HMI tags to 250ms? i cant find that function in the general setting of the tags. Im using Tia Portal 15.1 with Wincc Professional. The other thing is, when i go to the menu, u can find the logging tags options, which is like historical data, there im able to change the archive and acquisition cycles to 500ms (no less), but how can i read that data? All of this is because i want to read varaibles values at 250ms and introduce them in an SQL data base with a Visual Basic Script, but the Scada is just letting me introduce data at 1 second. Im young working with this program so if u help me i will be very greatfull. Thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/28/2022 11:16:36New subject after splitting |
|
3/28/2022 11:17 AM | |
Joined: 6/19/2017 Last visit: 6/12/2024 Posts: 8140 Rating:
|
Closed cause question posted twice. The second thread with the subject The HMI tags cant be set to a less cycle than 1 second no? is published within the conference SIMATIC WinCC (TIA Portal). Jen_Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on