9/4/2017 3:33 PM | |
Joined: 8/3/2009 Last visit: 9/12/2025 Posts: 16409 Rating:
|
Hello Arasan you can use a batch file to start the "Autostart" when you wan to do and not automatically at Windows startup look in the following FAQ: https://support.industry.siemens.com/cs/ww/en/view/19249315 There you can see how to create a working Batch file. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
9/5/2017 7:09 AM | |
Posts: 310 Rating:
|
Dear Murof, Thank you very much for information .In that link for Auto start while system restarting only . In my case , to create an icon on the desktop to lunch the wincc RT . If that icon (like shortcut icon ) pressing mean directly open the Project runtime .! Kindly help this . With best regards, Arasan..
|
Last edited by: Arasan at: 9/5/2017 7:11:30 AM |
|
Follow us on