6/1/2023 6:26 PM | |
Joined: 7/19/2022 Last visit: 9/12/2024 Posts: 384 Rating:
|
Hello Vijeolook, I think there is no limitation as such. When I was a PLC programmer, I tried not to exceed 70% for two reasons: - One since the larger the program, the longer the cycle time can be. But this, as long as the cycle time is not an inconvenience for your application, is not a problem. - The second reason is that in PLCs where the load memory is located in the SMC, there may be a risk that there will not be enough space to carry out another download to the PLC if very large changes have been made. |
If this Information really helps, you could use the Rate function |
|
Follow us on