12/28/2015 8:54 AM | |
Joined: 8/25/2005 Last visit: 9/16/2025 Posts: 1162 Rating:
|
Hello techbro, the FB isn't part of a libary. It is published as an application example. Please check this document:
Good luck |
This contribution was helpful to
1 thankful Users |
12/29/2015 12:52 AM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
Hello, When you installing STEP7 then the question came up if you want to install the libarrys, if you didn't chose anything then they will be installed. Look for a library with the name: "Redundant IO CGP V52", there you will find the blocks FB450...453 and FC450...451. The block you are mentioning is from a example from internet. How do you read out the operating state and status of an H system? . |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on