10/11/2018 2:34 PM | |
Posts: 9 Rating: (0) |
Hello everybody, I'm trying to get some information form a TicNet having some JSON capability and Modbus TCP with a CPU 410-5H used alone. The TicNet is directly connected to the CPU via RJ45 port 0. I'm using Modbuspn block and configured it with the db_param but get A100 problem. i tried different ways but unsuccessfully... The TicNet has a "slave" address (80), i don't find where to define it. IP of CPU : 140.80.0.3 IP of TicNet : 140.80.0.4 I suppose doing it wrong as i can reach what i want from a software (Modbus doctor), i give you the connections information to compare to my setup in PCS7. Every help would be much appreciated. Regards. AttachmentTicNet.zip (376 Downloads) |
Last edited by: UR85 at: 10/11/2018 2:36:48 PM |
|
10/12/2018 8:47 AM | |
Posts: 3093 Rating: (322)
|
Hello, Regards, |
This contribution was helpful to2 thankful Users |
10/17/2018 9:01 AM | |
Posts: 3093 Rating: (322)
|
Hello, Regards, |
10/17/2018 12:00 PM | |
Posts: 3093 Rating: (322)
|
If you attach an online print of the Modbus IDB as PDF file, I can take a look at it. Regards, |
Follow us on