9/9/2018 8:28 PM | |||||||
Joined: 3/12/2015 Last visit: 7/17/2024 Posts: 533 Rating:
|
Hello Daniel thank you for your response, as previously stated im using tiaportal v15 but ill link a picture so that you can see that it dosent let me add these devices together, also i have the cpu and the analogic module in my hands but the hole on the cpu is only on the left and the conector of the analogic module is also on the left |
||||||
9/9/2018 8:40 PM | |
Joined: 9/21/2012 Last visit: 7/25/2024 Posts: 4034 Rating:
|
You need something else than a C ended CPU, to be able to add the module? I think that the CPU you have chosen now, doesn't support additional I/O modules for the rack. |
This contribution was helpful to
2 thankful Users |
9/9/2018 9:11 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hello Jack, you cannot add SM module to 1211 CPU only one SB module
CPU 1211C - The clever compact solution • With 10 integrated inputs/outputs • Expandable by: - One signal board (SB) - Max. three communication modules (CM) • Three fast counters (100 kHz)
|
Last edited by: Ste39 at: 9/9/2018 9:15:00 PM |
|
This contribution was helpful to
1 thankful Users |
Follow us on