10/29/2015 9:23 AM | |
Posts: 8 Rating: (0) |
I am using the function MOVE_BLK_VARIANT and it works fine for native datatypes, like int, word, real and so on. But dosen't work for udt's. To me it seams to be a bug in PLC firmware, do anybody else had the same problem? PLC S7-1200, CPU 1212C ------------------------------------------------------------------------------------------ |
Last edited by: U_3e6b693f-92a5-4f36-9b0a-a4180640fded at: 10/29/2015 9:25:10 AMLast edited by: U_3e6b693f-92a5-4f36-9b0a-a4180640fded at: 10/29/2015 9:25:35 AMLast edited by: Min_Moderator at: 10/29/2015 6:38:39 PMNew subject after splitting |
|
11/3/2015 10:33 PM | |
Joined: 7/7/2010 Last visit: 6/4/2024 Posts: 14766 Rating: (2377)
|
Is your DB with the UDT set up as symbolic or absolute addressing? I think it needs to be absolute addressing for the MOVE_BLK_... to work. Check the documentation and / or readme files with the latest updates and SP1 to verify if the suggestion does not work out.
|
science guy |
|
Follow us on