2/7/2023 10:45 AM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi christopherreyes, have you tried tu upgrade the Library for PROFINET data records? This should be possible without any problems. The block "LPNDR_ReadMRPState" reads the MRP information from the MRP manager. You need to set the hardware ID of the PROFINET device, so you need to assign the SCALANCE to a PLC and use the instruction on that PLC. Kind regards |
This contribution was helpful to
1 thankful Users |
2/7/2023 11:21 AM | |
Joined: 1/10/2023 Last visit: 5/27/2025 Posts: 60 Rating:
|
Hi Stefan,thanks for your very quick answer. Omg I dind't know that the ".al16" file was a library... Okey now I have the library in my project but I don't know how to assign the SCALANCE to a PLC, I have some converters in my project and was quite easy assign it, for the SCALANCE seems is different, do you know how I can do? |
2/7/2023 9:50 PM | |
Joined: 9/27/2006 Last visit: 9/2/2025 Posts: 12397 Rating:
|
Hello christopher; I believe Stefan is refering to the rpRingState output in the LPNDR_ReadMrpState block. You can study the documentation on this block in the following FAQ: https://support.industry.siemens.com/cs/ca/en/view/109753067 Hope this helps, |
2/8/2023 7:47 AM | |
Joined: 1/21/2013 Last visit: 8/29/2025 Posts: 4087 Rating:
|
Hi christopherreyes,
the SCALANCE XC-200 devices have a signaling contact (see chapter 6.8 of operating instructions). You can wire this to an input channel of your PLC or any other suitable device. Kind regards |
This contribution was helpful to
1 thankful Users |
Follow us on