11/8/2022 9:39 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, Please refer SINUMERIK 840D sl Commissioning CNC: NC, PLC, Drive manual. 1. Refer chapter 6.3 Accordingly connect ALM & motor modules correctly. Connect Drive CLiQ cables properly. Go on line with STARTER & check the address. 2. Refer chapter 5 PLC Commissioning - accordingly modify PLC hard ware project as per devices connected, configure hardware address correctly & download PLC program. Check the hardware address alloted in PLC project & Sinamics drives matches or else fault/alarm message would triggered. 3. Please check max axes numbers to be configured to NCU & NX module, I guess max 6 for NCU & 6 nos NX module. 4. Refer chapter 6.4 Automatic device configuration with which you can configure Sinamics drives. Hope this helps. P. S. - Please note, to do so, all devices must be in working condition i.e. without any hardware fault.. |
Last edited by: Jen_Moderator at: 11/08/2022 10:47:20Link optimized. |
|
Follow us on