1/15/2016 3:15 PM | |
Posts: 163 Rating:
|
hello, as you can see from the screenshot, there is no ethernet no MPI on TIA PG/PC settings |
1/15/2016 3:31 PM | |
Joined: 5/12/2006 Last visit: 9/15/2025 Posts: 22710 Rating:
|
Hello, in windows Control panel a Item "PG/PC Settings" exist. If you open this are here the Interfaces displayed? Ín the TIA Project tree is a entry "Online access" here all found interface listed, do you see here the Interfaces? If this all is not working then there is a problem with the Interface installation duríng the setup. You can try to reinstall the interfaces with the steps from this FAQ: https://support.industry.siemens.com/cs/ww/en/view/99005532 Regards Christoph |
Last edited by: ChristophD at: 1/15/2016 3:33:00 PM |
|
Follow us on