3/14/2015 3:12 PM | |
Joined: 9/27/2006 Last visit: 9/9/2025 Posts: 12401 Rating:
|
Hello Vithani; I do not consider myself a drives specialist, but I have worked in many projects in various industries.. This type of problem has happened to us before, and the most likely suspect would be harmonic distorsion. An AC drive is composed of 3 sections: an AC-DC converter, a DC bus, and a DC-AC inverter that generates the output variable frequency signal to the motor. The converter is basically based of a diode bridge and usually uses 6-pulse technology (6 diodes in the bridge), unless you are willing to pay for 12-pulse or even 18-pulse technology (which adds phase transformers to 2 or 3 6-pulse diode bridges). The 6-pulse entry to standard VFDs is common, and relatively cheap, but produces very powerful harmonics (especially the 5th and 7th harmonic signals can be very destructive) which are multiples of the carrier frequency of the diode bridge carrier; this, through the resonant effect, will allow this harmonic power to interfere with the original power source frequency.. These harmonics are reflected back at the power source and can damage the quality of power signals in all equipment that is connected I believe this is happening to the power circuit of the PLC in your application. The common solution to this problem, once proper grounding of all electrical equipment has been taken care of, is to add a harmonic filter (or line reactor) at the input of the power circuit of the drive, to lessen the power of the harmonics produced by the diode bridge of the drive. The link that follows shows a harmonic filter sold by Danfoss for its drives, look at the power spectrums shown on the second page to see how the harmonics can be attebuated. http://www.danfoss.com/NR/rdonlyres/2B4828C1-170E-4F5C-9631-D4D93DE0AACC/0/High_AHF_MO008A02.pdf Since I do not know the model and caracteristicss of the drive you use, I suggest you contact your Danfoss dealer to see what harmonic filter he would recommend in your case. But remember that many manufacturers provide harmonic filters, and yiou can select from any one, as long as their specifications meet your drives requirements. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 3/14/2015 3:13:24 PMLast edited by: dchartier at: 3/14/2015 3:36:59 PM |
|
This contribution was helpful to
1 thankful Users |
Follow us on