7/21/2021 10:38 AM | |
Joined: 2/10/2015 Last visit: 11/10/2023 Posts: 7 Rating: (0) |
Hi, I am back working on my automation project, using the Openness api with python. The code was only slightly modified since I successfully used it before with V16Upd4. I've updated my Tia to V17.0 and created a new project with two PLCs, a CPU1516 and an old CPU317. The goal is to sequencially load different stations to both CPUs after their tasks have been completed. Right now, I am only able to successfully download a station to the CPU1516 after it has already been downloaded, not if there is currently a different project loaded (which makes the whole process pretty useless..) Downloading to the CPU317 doesn't work at all, no matter the prerequisites. My problem is that there is no indication to what is going wrong as the error message is completely useless to me. All the configuration options are done correctly, the delegates are used properly, so I am at a loss here. With the CPU1516, I think the newly added security features prevent me from properly downloading, but as there is no updated manual for openness (latest is for V16), I have nowhere to look for instructions how to handle that. I've added some screenshots, any help is much appreciated. AttachmentScreenshots.zip (126 Downloads) |
Last edited by: Jen_Moderator at: 07/21/2021 12:32:37Added embedded images as an attachment. |
|
Follow us on