5/6/2021 3:08 PM | |
Joined: 10/10/2005 Last visit: 1/29/2025 Posts: 1940 Rating:
|
Hello HaPeSoft, if the module 6ES7 SIM-01500-APLC is not compatible, can you delete this module in the hardware configuration? And start the simulation without this module. When modules are not compatible, the communication can not be started. See also the information of the FAQ: How do you start S7-PLCSIM in STEP 7 (TIA Portal)? With best regards |
4/1/2022 4:54 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating:
|
Same problem with v17, how did you solve it? |
This contribution was helpful to
1 thankful Users |
2/26/2023 3:07 AM | |
Posts: 1 Rating:
|
Gracias por su ayuda, tuve el mismo error y al cambiar la instancia a ET200SP se arreglo el problema |
11/6/2023 4:58 PM | |
Posts: 2 Rating:
|
I actually think since Update 1 the PLC Type dropdown is not working properly. I would think there would be many more posts about the issue. |
Follow us on