3/25/2021 3:31 AM | |
Joined: 10/17/2007 Last visit: 6/6/2024 Posts: 4002 Rating: (347)
|
Today I will update this topic with some questions--also any members if interested in it you can try to answer.--my target is " POST PICTURES--that will help me to understand your question" That is the real case of my customer, who came from my old customer recommendation: During COVID-19 pandemic --I normally don't travel to the customer site unless it is necessary. This customer is 200KM from me away, and he had a defective 810D machine system, I let him sending CCU and HMI (MMC103 and OP032 to me. I fixed the CCU lost communication issue and download NC/PLC back up from MMC103 to CCU (V1.6 very old). you as there are not motors and no encoder cables of course there is error LED "SF" on CCU and as there is no PLC I/O connected to CCU, there are 2 red LED's of PS and PF. I suggest the customer pick up the CCU and MMC, told them to connect carefully to the machine, and if they have a problem running--inform me. They did as I said. after 2 days, they sent me cell phone text, saying the machine not running error "axis not ready" I told them --please send a picture of MMC with alarms and picture of your CCU front and drive power supply.here is the MMC picture. and I will post CCU front picture in the next page. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 03/26/2021 07:55:13New subject after splitting Last edited by: Jen_Moderator at: 03/29/2021 09:09:10Optimized headline. If you like my comments please |
|
Follow us on