1/4/2023 3:07 PM | |
Joined: 6/24/2015 Last visit: 8/27/2025 Posts: 9 Rating:
|
Is it possible? |
1/4/2023 4:01 PM | |
Joined: 9/27/2006 Last visit: 9/11/2025 Posts: 12407 Rating:
|
Hello S7_Pseudonym; The S7-1500 communication manual contans this information (see the screenshot below) on IEEE 1588-based PTCP protocol over Profinet: https://support.industry.siemens.com/cs/ca/en/view/59192925 It looks therefore that Siemens developpers have considered the integration of Precision Time Protocol with S7-1500 PLCs. However, the PTCP description only descibes the configuration that would b necessary to implement it, and there are no FAQs or Application notes in SIOS giving specific descritions of PTCP integration.. If you want to research this further I would recommnd starting a Support Request (link at the top of this page) so that you can ask a Siemens communications specialist for more information. Hope this helps, |
This contribution was helpful to
3 thankful Users |
Follow us on