4/2/2020 5:16 PM | |
Joined: 4/2/2020 Last visit: 1/30/2025 Posts: 4 Rating:
|
Hello, i have a problem about WinCC Unified. When i start simulation of WinCC Unified RT, i got an error :"No start screen found". This issue arrives after placing of dynamic widgets in some screens (Not Start screen). Initially, the previous project was working perfectly. So, I have deleted those dynamic widgets and ensured the configuration of Start screen in the runtime settings but the same issue persist. Please help me to solve the issue. Thanks ! ------------------------------------------------------------------------------------------ |
Last edited by: DP89 at: 04/02/2020 17:18:51Last edited by: DP89 at: 04/02/2020 17:20:39Last edited by: Jen_Moderator at: 04/03/2020 07:44:40New subject after splitting |
|
12/6/2024 9:41 AM | |
Joined: 8/3/2009 Last visit: 9/2/2025 Posts: 16290 Rating:
|
Hello does it only appear in simulation or also if you start a runtime project in Runtime manager? does it only appear with a specific project or also with a new test project? Check if you have set upd your station correctly: https://support.industry.siemens.com/cs/de/en/view/109806850 Bye Murof |
If this Information really helps, you could use the Rate function |
|
4/16/2025 8:33 AM | |
Joined: 1/13/2020 Last visit: 7/18/2025 Posts: 13 Rating:
|
I have this problem with TIA V20 Upd. 1. Panel image is V20. I get both "No start screen was found" and "Error loading the screen". Happens somewhat randomly when navigating through screens. Edit: Seems the issue was solved after updating bootloader of the panel, I had a very old version of it on the Unified Comfort panel. Bootloader Update for SIMATIC HMI Unified Comfort Panels https://support.industry.siemens.com/cs/ww/en/view/109973587 |
Last edited by: IBFilter at: 04/25/2025 09:51:19 |
|
Follow us on