1/16/2023 9:03 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
yes without a PLC you can't use only the ET200S. The only tool which can be used for io-check without PLC is Proneta |
This contribution was helpful to
1 thankful Users |
1/16/2023 9:27 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
i think on the Microbox some Soft SPS is installed (WinAC, RTX) or? |
1/16/2023 9:45 AM | |
Joined: 5/12/2006 Last visit: 9/2/2025 Posts: 22709 Rating:
|
ok then you have programmed a PNIO Controller on the Microbox then you must do the same on your testsystem. |
Follow us on