4/18/2016 7:54 AM | |
Joined: 8/27/2006 Last visit: 10/22/2024 Posts: 719 Rating:
|
It seems that you won't be able to upload the backup because it does not exist. To have a backup stored on the HMI you should've selected the option "enable back transfer", which appears that you did not. You can only upload an image file using PROSAFE and re-download it to another similar HMI. Check this link for more details about back transfer |
Last edited by: AMAZINGAHMED at: 4/18/2016 7:55:58 AMThe more you know, The more you know that you don't know |
|
This contribution was helpful to
1 thankful Users |
4/18/2016 11:11 AM | |
Joined: 11/18/2010 Last visit: 8/5/2022 Posts: 523 Rating:
|
in addition to this i would like to share one thing is you cannot modify HMI on uploaded backup ,you just can load this to related HMI . Viral. |
4/18/2016 11:18 AM | |
Joined: 11/29/2014 Last visit: 9/13/2024 Posts: 96 Rating:
|
Viral Is it possible to get hmi backup without ticking backtransfer? |
4/18/2016 11:50 AM | |
Joined: 7/24/2014 Last visit: 8/1/2025 Posts: 393 Rating:
|
Dear dhaval In siemems uptill now without checking up the back transfer it's not possible to get complete upload of hmi And only possibility is of non editable image file |
Thanks and Regards |
|
4/18/2016 11:58 AM | |
Joined: 11/29/2014 Last visit: 9/13/2024 Posts: 96 Rating:
|
What if my HMI panel is obsolete and i want to transfer its backup to successor device .. Does it works? |
Last edited by: Dhaval Abotiyawala at: 4/18/2016 11:59:11 AM |
|
4/18/2016 12:02 PM | |
Joined: 7/24/2014 Last visit: 8/1/2025 Posts: 393 Rating:
|
Nope not possible |
Thanks and Regards |
|
4/20/2016 12:35 AM | |
Joined: 5/28/2008 Last visit: 9/3/2025 Posts: 4522 Rating:
|
Hello, Normally when you enable back transfer option, you need an external memory to save the project on it. Did you checked that the SIMATIC Panel does not have a memory card installed. If you have this memory card, it may be stored on it. If you don't have the editable backup, you can take non-editable image using prosave and you can download it to another Panel with the same Part number. And if your Panel became obsolete, You can still buy it from Siemens as Spare Parts or from other suppliers, there are hundreds online. Hope this helps. |
Ayman Elotaify |
|
Follow us on