1/12/2023 2:35 PM | |
Joined: 7/19/2022 Last visit: 9/11/2025 Posts: 436 Rating:
|
Hi AutoGen_3903701, You can have two HMI panels connected to the same PLC and accessing the same variables, but you have to create two different communication links. That is, each panel has to have its own IP address, PROFINET name or MPI name... depending on the communication protocol you use. |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
1/18/2023 10:17 AM | |
Joined: 9/1/2022 Last visit: 2/28/2023 Posts: 2 Rating:
|
Thanks. |
Follow us on