9/10/2020 12:10 PM | ||
Joined: 9/30/2016 Last visit: 5/23/2024 Posts: 912 Rating: (6) |
Hi PHS, That is really annoying (but I can see that it worked for naldi). What is the easiest way to get a 7.2 version? Do I really need to get hold f a WinCC v7.2 disk and make a complete installation (and I since I cannot "downgrade" from 7.4 to 7.2 I have to start on a fresh install of Windows as well)? Is WinCC 7.2 compatible with Windows10? Is WinCC 7.2 compatible with Windows7?
------------------------------------------------------------------------------------------ |
|
Last edited by: Jen_Moderator at: 09/10/2020 12:54:12New subject after splitting |
||
9/10/2020 2:26 PM | |
Joined: 10/10/2014 Last visit: 5/17/2024 Posts: 1725 Rating: (209) |
Hi xmnj, WinCC V7.2 is not compatible with Windows 10 WinCC V7.2 is compatible with Windows 7 See Kompatibilitäts-Tool für Automatisierungs- und Antriebstechnik https://support.industry.siemens.com/cs/ww/de/view/64847781 Best regards schufri |
This contribution was helpful to1 thankful Users |
9/11/2020 8:36 AM | ||
Joined: 9/30/2016 Last visit: 5/23/2024 Posts: 912 Rating: (6) |
Thank you for answering schufri, So the smartest way to get it done is to try to migrate in one step from 7.0 to 7.5 - as the manual says should be possible - but if that results in too many errors to "bite the bullet" and install 7.2 and do the migration in 2 steps. First 7.0 > 7.2 and then 7.2 > 7.5? "According to Migration Manual
" |
|
Follow us on