2/1/2023 2:09 PM | |
Joined: 11/29/2018 Last visit: 4/23/2024 Posts: 12 Rating:
|
Hi Why cant i chose the Ramp Function? Br Kasper |
Last edited by: kaan86 at: 02/01/2023 14:19:05 |
|
2/1/2023 6:34 PM | |
Joined: 3/30/2020 Last visit: 9/12/2025 Posts: 5446 Rating:
|
There is an application example that has the ramp function. See [With STEP 7, how can you control servovalves, frequency converters or current converters via a ramp-function generator?] Updating the PLC firmware to V4.2 (or V4.3 or V4.4) is a good idea for other reasons. One of those is that ,ore memory is made available for the program to use. The update can be done by the software but you have to download the firmware file from Siemens' support site. [Firmware version V4.2 released for S7-1200 CPUs] Do make sure that your version of software have the firmware versions in the hardware catelog before making an update. Is your problem resolved? |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
1 thankful Users |
2/2/2023 8:42 AM | |
Joined: 3/11/2019 Last visit: 9/1/2025 Posts: 1653 Rating:
|
At least upgrading to the lastest firmware is recommended from Siemens and is most likely also the first thing recommended from support, if there are any issues. If it is "useful" may be a different story. Firmware update for CPU 1215C, DC/DC/DC, 14DI/10DO/2AI/2AO"When updating the firmware, always update to the latest version available for the product and its respective article number" -> "V4.6.0" -> "Recommended for upgrade" regards sancruz |
Last edited by: sancruz at: 02/02/2023 08:49:45Feedback appreciated, please rate |
|
2/2/2023 3:17 PM | |
Joined: 11/29/2018 Last visit: 4/23/2024 Posts: 12 Rating:
|
Hi I updated the firmware and it works now thanks:) Br Kasper |
This contribution was helpful to
1 thankful Users |
Follow us on