3/27/2024 8:13 PM | |
Joined: 4/28/2015 Last visit: 8/5/2025 Posts: 6 Rating:
|
Hello everyone. Let me explain: Every time a popup is opened in Tia Unified, the popup receives a unique name. This unique name is composed of the prefix "FaceplatePopupWindow" plus a random number, for example, "FaceplatePopupWindow_192". Every time the popup is closed and opened again, the popup will receive a new unique name, even if it is the same popup. As this name is random I would like to read the name of this new opened popup and display it in a text box in the opened popup. The attached image shows an illustration of the case. We can see the popup open and the diagnosis saying that it was not possible to read the name of the popup. It is possible to see in the diagnostics that the system took the name of the opened popup (in this example, the name of the opened popup is "FaceplatePopupWindow_228"). Below, in Chrome debugging mode, it is possible to see this popup property opened according to the SIEMENS FAQ: https://support.industry.siemens.com/cs/ww/en/view/109810540 Lastly, I've already tried a number of different ways. I ask for help from a specialist to help me with this difficulty. |
Last edited by: Jen_Moderator at: 03/28/2024 09:24:29Text formatting and link optimized. |
|
Follow us on