10/12/2021 4:35 PM | |
Joined: 8/1/2012 Last visit: 7/30/2023 Posts: 178 Rating: (15) |
hi guys, can anyone help me with telling the source of the dynamic address in PLC alarm window in HMI please?? (look at the attached) I've already changed the PLC address of rack 1 in H-station in both simatic manager and HMI (in TIA portal in connection editor and also in VBS script ) but the redundancy is not ok and if I stop the cpu0 the HMI loses connection with H-Station, also the alarm window comes up and shows the former IP address which I changed any further information is needed tell me to add by the way I followed the bellow instruction to establish redundant connection with H-station https://support.industry.siemens.com/cs/ww/en/view/96837136 best regards Mojtaba AttachmentDoc1.pdf (142 Downloads) |
|
|
Follow us on