9/27/2018 11:10 AM | |
Posts: 3 Rating: (0) |
Dear All, In one of our project, I need to communicate with 6 nos. of S7-1200 PLC (6ES7-212-1BE40-0XB0) from GE RX3i redundant system using PROFINET protocol. The S7-1200 PLC is used as Profinet IO device (slave) and GE PLC Profinet Controller (IC695PNC001) is used as Profinet IO Controller (master). Please refer attached architecture. Can someone confirm whether this architecture is valid or not? We are facing problem that the S7-1200 PLC are communicating with GE Primary PLC only and not communicating with secondary PLC. The S7-1200 PLC GSDML file doesn't have 'system redundancy' option. We are able to map the GSDML file to Primary GE PLC only and NOT able to map to Secondary GE PLC. So only Primary GE PLC is communicating with S7-1200 PLC. So now I have doubt on this Profinet Architecture. Thanks, Ketu Parikh AttachmentProfinet System Architecture.ppt (507 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on