1/1/2016 2:41 PM | |
Posts: 113 Rating: (1) |
Hello everyone... I have a probleme with S7 Simulator. It dosn't work. Any help ? Best regards |
1/1/2016 2:59 PM | |
Posts: 113 Rating: (1) |
download it from the net...Can I put the link here? |
1/1/2016 4:00 PM | |
Posts: 113 Rating: (1) |
yep I think that the link is illegal. I will try to download another one and we'll see... thank you alot Sir |
1/1/2016 5:52 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, OFT Please do not hesitate to write any issue here. The meaning of forum is discussion - questions and answers. Just give more details and specify the problem. Back to your questions: Simulator in case of S7-200 - please search for it here in forum. A lot of discussions without any positive result. Personally I am testing S7-200 software in PLCSIM (the tool for S7-300 and S7-400 hardware). Unfortunately it is not just copy and paste the code because of differences in syntax. S7-200 and HSC - https://support.industry.siemens.com/cs/us/en/view/27864874 (It is just to start up). Best regards, Hristo Mihalev |
Last edited by: UMENCHO at: 1/1/2016 5:53:43 PM |
|
This contribution was helpful to1 thankful Users |
1/1/2016 8:32 PM | |
Posts: 113 Rating: (1) |
I'm using S7 200 -CPU 224 there is one port 485 so I use profibus to connect it to the panel... and this is th configuration in wincc... |
Follow us on