6/22/2017 10:33 AM | |
Posts: 3 Rating:
|
Hi, My project using Unidrive M701 Emerson, PLC S7-200 CPU226 and HMI WINCC Flexible 2008. The problem is the motor speed value not displaying in the HMI. Previously it's works well with Unidrive SP1401 before migrate to M701. With Modbus rtu communication, the address of the drive parameters change (now parameters are 1.001 instead of 1.01 for example and some of them are different between SP1401 and M701. Does it effect the PLC S7200 from receiving the data? Here i attached SP1401 and M701 parameters file. AttachmentSP1401 and M701.pdf (950 Downloads) |
Last edited by: NORLIZA at: 6/22/2017 10:35:33 AM |
|
Follow us on