9/2/2014 12:49 PM | |
Joined: 1/28/2009 Last visit: 8/31/2025 Posts: 6874 Rating:
|
Hello, It is possible to converst SCL codes from STEP 7 V5.5 to an executable version in TIAV12 with the following tool:
Wizard for converting SCL source files from V5.x to V1x I can not guess the problem without checking your original STEP 7 project.If you have a consistent project in STEP 7, you can migrate it to TIA Portal version if you have both softwares at a same system. If this is not possible, try to recreate same situation with making a source file from elements inside the FB.Start from generating elements such as UDT and develop to other blocks. I hope this helps, Hamid Hosseini |
This contribution was helpful to
1 thankful Users |
Follow us on