4/7/2017 7:58 PM | |
Posts: 1 Rating:
|
Hola buena tarde, tengo problemas para configurar un sinamics s110 para un plc 1500, como se que telegrama asignarle?? y tambien si el STARTER tiene problemas con Windows 10 ya que se reiniciana en cuanto quiero comunicarme con mi S110 ----------------------------------------------------------------------------- Hello good afternoon, I have problems setting up a sinamics s110 for a 1500 plc, how do I know which telegram to assign it ?? And also if the STARTER has problems with Windows 10 and it will restart as soon as I want to communicate with my S110 ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/10/2017 12:46:50 PMAdd translation Last edited by: Min_Moderator at: 4/10/2017 12:47:16 PMNew subject after splitting |
|
4/11/2017 11:00 AM | |
Joined: 10/11/2006 Last visit: 9/15/2025 Posts: 6040 Rating:
|
Hello, you must use GSD with Telegram 3 or 5 for S110. https://support.industry.siemens.com/cs/de/en/view/73257075 The connection with TO is like S120. https://support.industry.siemens.com/cs/ww/en/view/109482718 |
With best regards, |
|
Follow us on