6/2/2014 8:58 AM | |
Joined: 4/19/2008 Last visit: 6/25/2024 Posts: 1525 Rating: (159) |
Hello WaelRamadan, You need a Step 7 Basic or Step 7 Profasional..... What are the essential differences between STEP 7 Lite and STEP 7 / STEP 7 Professional? Which SIMATIC software packages are compatible with which Microsoft Windows operating system and with STEP 7 V5.5? Which SIMATIC software can you install in 64-bit operating systems? |
Last edited by: Ammy at: 6/2/2014 9:01 AMAmmy |
|
6/2/2014 11:21 AM | |
Joined: 11/21/2007 Last visit: 7/7/2024 Posts: 2325 Rating: (307) |
Hello WaelRamadan If you have a Simple S7-300 System ( WIthout any special modules like CPs / FMs etc ) , then you can use the STEP-7 Lite Free Download software from the following link : STEP 7 Lite available for downloading For communicating with the S7-300 CPU, if you have a CPU with PN ( EThernet ) interface, then you do not need any special cable. Just a CAT5 CAT6 cable would do. If you have a CPU with MPI / Profibus Ports only the you would need a PC UCB Adaptor |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
2/19/2015 9:53 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating: (123) |
|
Follow us on