12/8/2020 7:16 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Hello, You should have post this topic in SINUMERIK CNC automation systems product conference. BTW is it running old machine or new under commissioning? If it is old machine. check value in r036 & fault value in r0949. This is calcualted basec on I2T formula, so check the current drawn by motor, also check motor, motor power connector any loose connection etc. etc. Check power module value in r207 & compare with r036. If it is new machine under commissioning, check drive commissioning & motor identification. HTH |
This contribution was helpful to
1 thankful Users |
Follow us on