5/30/2008 10:04 AM | |
Joined: 4/23/2008 Last visit: 8/20/2025 Posts: 12 Rating:
|
Hi, the actual version of Sizer is V2.9. Try to get this new version and it should be ok. |
11/10/2012 3:43 AM | |
Posts: 1 Rating:
|
Hi ! everyone. You expereiced the problem as I did. When I tried to use SIZER 3.7 HF1, I got stuck waiting for loading SIZER and just saw this message. "Connection to the currently selected database has failed" I installed SIZER 3.7 again. It looked fine first. However, when I rebooted laptop, I was back to square one. So, I considerred what the database in SIZER is. Database in SIZER is based on SQL Server. I assumed there is connection problems between laptop and SQL Server. So, I installed Microsoft SQL Server 2008 program; It requires Microsoft Windows Installer 4.5. STEP 1) Install Microsoft Windows Installer 4.5, if you don't have it. STEP 2) Install Microsoft SQL Server 2008; I selected upgrade option from SQL Server 2000/2005. STEP 3) In Windows, loadSQL_Server_Configuration_Manager Now you are ready to adjust SQL Server Configuration In SQL Server Configuration, STEP 4) Search properties of SQL Server (SQLEXPRESS) in SQL_Server Services STEP 5) In Service tab, Start Mode = Automatic STEP 6) In Log On tab, Built-in account = Local System STEP 7) In Log On tab, Service status >> Click "Start" icon. I hope you solve the problem of loading SIZER. Please refer to attached pics in zip file. Have a good day ever and ever. AttachmentSQL_Server_Configuration.zip (570 Downloads) |
Last edited by: Nimrod_K at: 11/12/2012 12:49 AMLast edited by: Nimrod_K at: 11/10/2012 3:57 AMLast edited by: Nimrod_K at: 11/10/2012 3:56 AMLast edited by: Nimrod_K at: 11/10/2012 3:44 AM |
|
This contribution was helpful to
1 thankful Users |
Follow us on