4/24/2017 12:36 PM | |
Joined: 7/2/2008 Last visit: 8/7/2025 Posts: 928 Rating:
|
Hello Soonseng, As far as I remember, you can't use the CP343-1 Lean to establish a redundant link. The lean version doesn't support ISO connections. You can use it for HMI/SCADA connection. The redundant link can be established over Ethernet (ISO connection), Profibus (FDL connection) and MPI (Non configured connection). Even the integrated PN ports will not help as they do not support ISO connections. The only way is to use CP343-1 (6GK7343-1EX30-0XE0)
It means to link stations to Ethernet networks but not for redundant links. I know this part is deceiving. Best regards, H-H |
5/8/2017 12:07 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4759 Rating:
|
New question published by K110586 is split to a separate thread with the subject Software redundancy link with MPI. Best regards |
Follow us on