12/15/2010 7:15 AM | |
Joined: 8/10/2006 Last visit: 2/13/2025 Posts: 156 Rating:
|
Hi, I am also not an expert. But I use PG-USB cable AG150. www.tpa-partner.de/kabel.htm Regards, Raheel |
12/15/2010 2:45 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Perhaps this FAQ might clarify the problem - System message no. 0334" when attempting to go online with STEP 5 V7.2 in Windows XP Best regards, Hristo Mihalev |
12/15/2010 5:46 PM | |
Joined: 9/27/2006 Last visit: 9/16/2025 Posts: 12408 Rating:
|
The help that members here have been giving you relates to Step 5, and there might be differences in the way a 3rd-party sets the communications parameters for their software. This is the site of the developpers of PG2000: http://www.process-informatik.de Maybe you should contact them at this point, or look at their documentation. Hope this helps, Daniel Chartier |
1/15/2011 8:03 PM | |
Posts: 2 Rating:
|
Some times the Port in the 95 U is faulty so it is as good as not connecting check it.get it re[paired some opto Ics are there.Regards Narang Bhagwati Automation |
Follow us on